Issue:
Part number for remote mount keypad for the ATV12.
Product line:
ATV12, Altivar 12
Environment:
All serial numbers
Cause:
N/A
Resolution:
There are two keypad options: VW3A1006 (IP54) or the VW3A1007 (IP65).
The kit comes with the screws to mount the keypad to an enclosure or door. A cable to connect the keypad to the drive is not included. Customer needs to order cable VW3A1104R10 (1 meter) or VW3A1104R30 (3 meter) separately.
Part number for remote mount keypad for the ATV12.
Product line:
ATV12, Altivar 12
Environment:
All serial numbers
Cause:
N/A
Resolution:
There are two keypad options: VW3A1006 (IP54) or the VW3A1007 (IP65).
The kit comes with the screws to mount the keypad to an enclosure or door. A cable to connect the keypad to the drive is not included. Customer needs to order cable VW3A1104R10 (1 meter) or VW3A1104R30 (3 meter) separately.
Released for:Schneider Electric Global