{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What's the difference between the 3 ATV312 display LED's flashing and scrolling?
Issue:
Looking for the difference between the 3 ATV312 display LED's flashing and scrolling?

Product Line:
ALTIVAR 312

Environment:
All

Cause:
Installation / Setup

Resolution:
Scrolling LED's mean that the drive is in Local mode (full control with the face of the drive unless programmed otherwise).
Flashing LED's at the same time mean the drive is in Local programming mode. The drive will not accept a run command in this mode.
If all three LED's are off or just one is lighted, the drive is in remote mode.

See this article for more in-depth details.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Global