Issue:
Why does my drive show Obr on display when ramping down on ATV61 or ATV71?
Product Line:
ATV61, ATV71, Altivar 61, Altivar 71
Environment:
All
Cause:
N/A
Resolution:
Obr [Overbreaking] is a drive state and not a fault. It is displayed in the top left corner of the graphic keypad if the drive is decelerating and using the Auto-Adapted Deceleration Ramp to avoid a possible overbreaking fault (ObF). This status may show up when Decel Ramp Adapt parameter is enabled.
Why does my drive show Obr on display when ramping down on ATV61 or ATV71?
Product Line:
ATV61, ATV71, Altivar 61, Altivar 71
Environment:
All
Cause:
N/A
Resolution:
Obr [Overbreaking] is a drive state and not a fault. It is displayed in the top left corner of the graphic keypad if the drive is decelerating and using the Auto-Adapted Deceleration Ramp to avoid a possible overbreaking fault (ObF). This status may show up when Decel Ramp Adapt parameter is enabled.
Released for:Schneider Electric Global