{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What versions of the ATV32 Drive is the Profinet card compatible with?
Issue:
ATV32 Drive Profinet card

Product Line:
ATV32, Altivar 32

Environment:
All

Cause:
N/A

Resolution:
The VW3A3627 option module is compliant with Altivar 32 with versions of V1.8 IE11 or higher.