Issue
Is it possible for a Magelis / Harmony HMI to communicate to a M241 Serial Line 2 via SoMachine / Machine Expert protocol?
Product
EcoStruxure Machine Expert
SoMachine
Harmony HMI
Modicon M241 PLC
Environment
HMI and PLC programming software for Windows
Physical communication between devices
Resolution
Yes, the M241 can communicate to an HMI via SL2.
The default communication settings for SL2 does not match the settings for the COM of the HMI (baud rate and parity are different). If the settings are adapted, the communication works fine.

Below is the RS485 pinout:
HMI to M241 SL2
Pin 4 to D1
Pin 5 to D0
Is it possible for a Magelis / Harmony HMI to communicate to a M241 Serial Line 2 via SoMachine / Machine Expert protocol?
Product
EcoStruxure Machine Expert
SoMachine
Harmony HMI
Modicon M241 PLC
Environment
HMI and PLC programming software for Windows
Physical communication between devices
Resolution
Yes, the M241 can communicate to an HMI via SL2.
The default communication settings for SL2 does not match the settings for the COM of the HMI (baud rate and parity are different). If the settings are adapted, the communication works fine.
Below is the RS485 pinout:
HMI to M241 SL2
Pin 4 to D1
Pin 5 to D0
Released for:Schneider Electric Global