According to our voltage tolerance design rule, the allow tolerance of DC products is around 85% to 120%. the allow voltage range of AC products is around 90Vac ~ 264V ac, if the supportable AC voltage is 110Vac and 240Vac in our catalog.
Released for:Schneider Electric Global