{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why there is no Test Certificates available for Easypact MVS / CVS in BlokSeT Evo?

Article available in these languages: Turkish

Easypact MVS / CVS is not tested in BlokSeT because,
  • The dimension and mounting of the MVS / CVS is exactly identical to NW or MTZ / NSX.
  • Thermal characteristics, power loss and current path of MVS / CVS is same with the tested design of NW or MTZ / NSX.
  • The short circuit rating of the MVS / CVS is less than Blokset Icw
In this situation, as per the below clauses of IEC 61439-1 :2011 the BlokSeT with MVS / CVS complies to IEC 61439-1 & 2.