{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Do M221 controllers have CANopen communication?
M221 controllers do not have CANopen communication.

If a customer needs CANopen communication, he will have to use at least a M241 controller. M241 controllers use Machine Expert software (previously called SoMachine), a different software than the Machine Expert Basic (previously called SoMachine Basic) that M221 controllers use.. Machine Expert Basic projects can be imported in a Machine Expert project easily.