Issue:
Maximum available current on ATV12 Drive 24Vdc Power Supply
Product Line:
ATV12, Altivar 12
Environment:
All
Cause:
N/A
Resolution:
Maximum customer current available is 100 mA (+ 24 VDC -15% +20% protected against short-circuits and overloads).
Maximum available current on ATV12 Drive 24Vdc Power Supply
Product Line:
ATV12, Altivar 12
Environment:
All
Cause:
N/A
Resolution:
Maximum customer current available is 100 mA (+ 24 VDC -15% +20% protected against short-circuits and overloads).
Released for:Schneider Electric Global