{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Unable to add data log viewer to a Vista diagram

Issue
When attempting to add additional data log viewers to a Vista diagram, the diagram will not save.

Product Line
Power Monitoring Expert 8.1

Environment
Vista

Cause
The diagram has reached the maximum number of data log viewer objects allowed.  This limit is 60 data log viewer objects per diagram.

Resolution
1.)Apply hotfix available at FA293828 that increases the limit from 60 to 100 data log viewer objects per diagram.

2.) Install service pack 2 to bring the system up to PME 8.2

3.) Upgrade to PME 9.0. Please contact Technical Support for purchasing options.


Schneider Electric Global