Issue:
Keypad compatibility with the Altivar 320.
Product Line:
Altivar 320
Environment:
All serial numbers for Altivar 320
Cause:
N/A
Resolution:
The Altivar 320 drive is compatible with the list of keypads:
The ATV61/71 keypad requires mounting kit VW3A1102 (provides for IP54, add VW3A1103 for IP65).
Cables must be ordered separately
Keypad compatibility with the Altivar 320.
Product Line:
Altivar 320
Environment:
All serial numbers for Altivar 320
Cause:
N/A
Resolution:
The Altivar 320 drive is compatible with the list of keypads:
- VW3A1111 (Altivar Process Drive keypad)
- VW3A1101 (Altivar 61/71)
- VW3A1006 (ATV312/32 keypad - IP54)
- VW3A1007 (ATV312/32 keypad - IP65)
The ATV61/71 keypad requires mounting kit VW3A1102 (provides for IP54, add VW3A1103 for IP65).
Cables must be ordered separately
- VW3A1104R10 - 1 Meter Cable
- VW3A1104R30 - 3 Meter Cable
- VW3A1104R50 - 5 Meter Cable
- VW3A1104R100 - 10 Meter Cable
Released for:Schneider Electric Global