{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to use USB host port on SCADAPack 535E

How to use USB on SCADAPack 535E

The USB Host and USB Device ports on the SCADAPack 535E are USB 2.0-compliant ports that support 1.5 Mb/s and 12 Mb/s communications. The USB ports automatically detect and support the data rate of the connected device. The two USB ports can be used simultaneously.

The USB Host port is a USB series A receptacle that allows the rPAC controller board to act as a host for a plug-in USB drive. For bus-powered USB devices, the USB Host port can provide up to 100 mA at 5 Vdc.

The USB Host port is not user configurable. It can be mounted and accessed through the rPAC file system at /usb0.

Product Line

SCADAPack 535E

Environment

Windows OSes, Terminal

Resolution

Connect to SCADAPack 535E by using any Telnet client:

by issuing devinfo command you can obtain the information about available device drives:

And current directory can be changed by cd command.
If the USB Storage is not plugged or not ready Directory not available message will appear on the screen:

If USB Device is present, prompt will change to the following:

Then dir command can be used to get some information about the usb drive:

USB Storage can be used in Remote Command Line, Telnet and Workbench Logic and increase amount of space up to 32 GB. File System Format has to be FAT32.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.