{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why is the UPS thermal dissipation rating calculated using efficiency data different from the value specified on www.apc.com?
Issue:
The thermal dissipation rating specified on the APC website is sometimes different than the value calculated using efficiency data or the UPS Efficiency Comparison Calculator.

Cause:
The value calculated using efficiency data or the Efficiency Comparison Calculator is based on nominal environmental conditions (25C, 230V 50Hz input), in green mode with a fully charged battery.
The values on the web are specified for less-than-nominal environmental conditions, such as maximum charging power, active AVR, high ambient temperature, etc.

Resolution:
Both values are correct, depending on the circumstances. Calculated values are typical for nominal conditions, and the ones specified on the website apply for worst-case scenarios.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.