{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Loaded the EDS file for XPSMCMCO0000EI Ethernet IP but getting an error Incorrect Vendor Data. How to resolve the issue?
Issue:
Loaded the EDS file for XPSMCMCO0000EI Ethernet IP but getting an error Incorrect Vendor Data.  How to resolve the issue?

Product Line:
XPSMCM, SoSafe

Resolution:
This is a known issue, please see page 8 of attached document.

From that document: In the new XPSMCMCO0000EI  firmware V1.8 version for the Vendor data contents have been updated. The previous EDS - files are not in accordance with the new data. This incompatibility appears also in combination of latest EDS file with EIP communication modules having previous FW version. As a result, during setup of the communication, it is not allowed to use the feature "Electronic Keying" (Vendor data checking).To enable the communication with EIP communication module FW V1.8 it is mandatory to remove ticks from "Electronic Keying" check boxes  until EDS -file SE_ET_XPSMCM_0108E_20150916.eds in XPSMCM_Ethernet_EDS_V1_8_20150916.zip.

Schneider Electric Global

Attachment(s)
XPSMCM communication modules description_20150929.pdf [906.24 KB]
XPSMCM_Ethernet_EDS_V1_8_20150916.zip [17.96 KB]
Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: