Can you use one large line reactor on multiple drives vs one line reactor for one drive?
Published date:
04 January 2019
Issue:
Can you use one large line reactor on multiple drives vs one line reactor for one drive?
Product Line:
Altivar Drives
Environment:
All
Cause:
Would like to use only one line reactor and feed multiple drives.
Resolution:
No, it is best to have individual line reactors. If a single line reactor is used, it will have lower inductance and may not be enough if a single drive is running.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.