{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I configure WebReach for a 50 Hz system?
For PME 7.2.2 and PME versions prior to 7.2, WebReach requires an additional configuration step if the power system is not 60Hz (for example, 50Hz).  To do this, a user needs add or modify the registry key “LineFrequency” under the WebReach subdirectory of PME.  This key should be assigned a DWORD value of 50(or 0x32 hex) in the case of a 50Hz system.  This value will then be used by WebReach in the calculation of the RMS plot.

Taking PME7.2.2 for example,

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.