M580 CPU SD memory card format procedure
NOTE - Only use the BMXRMS004GPF SD card for the M580
NOTE - Only use the BMXRMS004GPF SD card for the M580
- Connect to M580 and make sure the Unity project is “Equal”, “Run” and “Built”
- Stop the PLC
- Open SD card door and make sure LED is ON
- Open the “Animation Table” Window
- Add system word %SW93.0 and %SW93.1
- Turn on the “Modification” button
- Enter value “1” for %SW93.0
- (This will start the format of the SD card then that value will change back to “0” and the value of %SW93.1 will go from “0” to “1” to indicate the format has completed successfully), (Formatting a standard SD card takes about 30-50 seconds)
- When completed, enter a value of “0” for both %SW93.0 and %SW93.1
- Start PLC
Released for:Schneider Electric Global