{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to uninstall Ecoreach if the uninstall is unsuccessful while uninstalling from control panel>Program and Features>Uninstall or change a program?
The “EcoreachUninstaller” is useful when there is a problem with ecoreach uninstallation. Usually, the ecoreach uninstallation problems occur when the Ecoreach.msi is not found or deleted from the computer which has ecoreach already installed.
For running this program on windows 10 and windows 8 remember to right click on the EcoreachUninstaller executable and select “Run as Administrator” option.
Here are the steps to be followed to uninstall Ecoreach using the “EcoreachUninstaller”: -
  1. Copy the “EcoreachUninstaller.exe” and “MicrosoftProgram_Install_and_Uninstall.meta” at the same location. (Zipped folder containing both the files are attached.)
  2. Execute the “EcoreachUninstaller.exe” by clicking the “EcoreachUninstaller.exe”.
  3. The command prompt will start, follow the instructions on the command prompt to uninstall ecoreach. (Computer may restart.)
  4. On the command prompt, the status of uninstallation will be displayed. (Uninstallation Successful!!!) or (Uninstallation unsuccessful!!!).
  5. Once the uninstallation is successful, ecoreach can be reinstalled.
Confirm the successful uninstallation from Control Panel => “Program and Features/Uninstall or change a program”.

Schneider Electric Global

Attachment(s)
Ecoreach_Uninstaller.7z [240.02 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.