{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is it possible to extend the distance between BCPM CTs and the adapter board?
It depends on which CT's your are referring to. The split-core branch CT leads can be extended to a maximum length of 6 meters without losing accuracy.
The 1VAC AUX CT leads can be extended to 30.5 meters.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.