Issue:
Set up the ATV320 drive so that the digital DO output controls output contactor command OCC.
Product Line:
ATV320
Environment:
All
Cause:
Wants to set up the DQ or DO so that it controls the a output for OCC.
Resolution:
Wiring:
Jumper +24vdc to DQ+
Wire your + side of your relay coil to DQ-
Wire the other side of the coil to Com
Programming:
In the Application Function Menu, set OCC to DO1
Set up the ATV320 drive so that the digital DO output controls output contactor command OCC.
Product Line:
ATV320
Environment:
All
Cause:
Wants to set up the DQ or DO so that it controls the a output for OCC.
Resolution:
Wiring:
Jumper +24vdc to DQ+
Wire your + side of your relay coil to DQ-
Wire the other side of the coil to Com
Programming:
In the Application Function Menu, set OCC to DO1
Released for:Schneider Electric Global