{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the Quantum 140NOE77101 hostname be changed?
Issue

Where the Host Name “140-NOE-771-01 Module” is being stored? Can it be changed?

Product Line

Quantum

Resolution

The Host Name “140-NOE-771-01 Module” is stored in the SNMP OID “System Name:” property.

The SNMP OID “System Name:” property is it read only, therefore, the hostname can’t be changed