{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the ATV212 or the ATV320 Drive accept multiple motor wires directly on its terminals or external terminals are required?

Article available in these languages: Spanish

Issue:
Does ATV212 or the ATV320 Drives accept multiple motor wires directly on its terminals or external terminals are required?

Product Line:
ATV320, ATV212

Environment:
All

Cause:
NA

Resolution:
It is not recommended to connect 2 motor wires to 1 drive's output terminal for ATV212 and ATV320. Need to do it externally.

Schneider Electric Global