{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
PM5560 that has stopped logging kWH on firmware 1.003
Product Line
PM5560

Environment
Logging

Resolution
This is an issue in the 1.x.xxx version of PM5500 firmware which was causing a File Status error condition and issue of occasional missing records in the data log. The device driver stops downloading on-board data logs after some time (approximately 2 months if the data logging interval is 15 minutes)

These issues have been fixed in FW V2.0.1. See Video: PowerLogic PM5500 - Upgrade Procedure for Firmware using FTP