{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
ATV320 Why can't I assign the logic inputs in the I/O menu?
Issue:
ATV320 Unable to change the logic inputs in the I/O menu.

Product Line:
ATV320

Environment:
All

Cause:
Programming logic inputs

Resolution:
You can not assign a function to the logic inputs in I/O menu.
Those are  read only parameters.
You must assign a logic input to the function you need.
Example, If you want to assign freewheel stop to LI2, you would need to go to CONF / FULL / FUN / STT, then go to NST and assign LI2 to NST.