Issue:
Why does the IP address reset back to all zeros after power cycling the ATV61/ATV71 VW3A3327 Profinet option card?
Product Line:
ATV61 and ATV71
Environment:
All
Cause:
Force to local is set
Resolution:
Check to see if force to local is turned on if so turn it off and use the ref and command switching in menu 1.6 and 1.7.
Why does the IP address reset back to all zeros after power cycling the ATV61/ATV71 VW3A3327 Profinet option card?
Product Line:
ATV61 and ATV71
Environment:
All
Cause:
Force to local is set
Resolution:
Check to see if force to local is turned on if so turn it off and use the ref and command switching in menu 1.6 and 1.7.
Released for:Schneider Electric Global