Issue:
How do I retrieve the value of a BOOL in a Vijeo Designer Script?
Product Line:
Vijeo Designer (all versions)
Resolution:
To retrieve the value of a BOOL in a Vijeo Designer Script, you need to use the following call:
Suppose we have a Vijeo Designer variable: BOOL01
The script call is:
BOOL01.getIntValue();
The result is going to be 0 or 1
To use the return value, you should declare an int and store the return value in it.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Global