Issue
How to make the cross reference window more user friendly.
Product Line
Unity
Environment
Windows 10
Resolution
When the cross reference window is opened, it appears as a small short window at the bottom of the Unity main window.
If there are a lot of variables, the user will need to scroll all the way down the window to find the variable. It could be much
easier to use as well as more user friendly, if the cross reference window can be opened in a larger window as the animation
table or logic window.

The following steps can be used to make the cross reference window more user friendly.
The Cross reference window will appear as a child window in the Unity logic workspace.

How to make the cross reference window more user friendly.
Product Line
Unity
Environment
Windows 10
Resolution
When the cross reference window is opened, it appears as a small short window at the bottom of the Unity main window.
If there are a lot of variables, the user will need to scroll all the way down the window to find the variable. It could be much
easier to use as well as more user friendly, if the cross reference window can be opened in a larger window as the animation
table or logic window.
The following steps can be used to make the cross reference window more user friendly.
- Right click on the top menu bar of the cross reference window.
- Click on 'MIDI child.
The Cross reference window will appear as a child window in the Unity logic workspace.
Released for:Schneider Electric Global