{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is the x80 I/O Class 1 Div 2 rated?
Issue:
Is the x80 I/O rated for hazardous locations?

Product Line:
x80 M340 M580

Resolution:
The Modicon x80 I/O is rated for hazardous location Class 1 Div 2 groups A,B,C,D in Canada and USA

82494_IMG