{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can you connect the remote HMI to the soft starter, ATS48 soft starter if you are using the RJ45 for a remote Ethernet gateway?

Article available in these languages: Spanish

Issue:
Connecting remote HMI to ATS48 while using the RJ45 for a remote Ethernet gateway.

Product Line:
ATV48

Environment:
All

Cause:
RJ45 ports limits when multiple options are needed.

Resolution:
You can only have one thing plugged into the RJ45 port at a time. There is no way to split the port and use both, one for HMI and one for Ethernet gateway.
One option is to use the remote HMI on the RJ45 port, and then use a Tesys T module to monitor motor amps and voltage etc.

Schneider Electric Global