Issue:
Need ATV61 and ATV71 basic integrated modbus setup assistance.
Product Line:
ATV61 and ATV71 standard internal modbus
Environment:
All
Cause:
Basic modbus setup assistance.
Resolution:
Programming: Menu 1.9
Modbus Network
Add- address set to 1 to 247
tbr= modbus baud rate choose 4.8, 9.6, 19.2 or 38.4K
tFO=Modbus format choose 8O1, 8E1, 8N1 or 8N2
ttO= modbus timeout set between 0.1 to 30 seconds.
You must now power cycle the drive and wait until the display goes out and then you can power it back up again after you change any of the modbus settings.
Wiring is pins 4 and 5 for data + and - and pin 8 for com
The wiring connection is a RJ45
Need ATV61 and ATV71 basic integrated modbus setup assistance.
Product Line:
ATV61 and ATV71 standard internal modbus
Environment:
All
Cause:
Basic modbus setup assistance.
Resolution:
Programming: Menu 1.9
Modbus Network
Add- address set to 1 to 247
tbr= modbus baud rate choose 4.8, 9.6, 19.2 or 38.4K
tFO=Modbus format choose 8O1, 8E1, 8N1 or 8N2
ttO= modbus timeout set between 0.1 to 30 seconds.
You must now power cycle the drive and wait until the display goes out and then you can power it back up again after you change any of the modbus settings.
Wiring is pins 4 and 5 for data + and - and pin 8 for com
The wiring connection is a RJ45
Released for:Schneider Electric Global