{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What tools can I use to transfer the ATVLogic programming?
Issue:
Customer wants to transfer the ATVLogic programming between ATV320 Drives

Product line:
Altivar 320, ATV320

Environment:
all

Cause:
n/a

Resolution:
ATVLogic can be transferred using Multiloader (V3.17 and higher) and Simpleloader (V1.7 and higher). You should be able to successfully transfer all ATV320 programming, including ATVLogic.

To be successful you have to ensure the drive is stopped and that the FB Status (FbSt) is Stop:
d

If the FB status is Run, you must change FB Command (FbCd) to Stop.
d

Schneider Electric Global