{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can a splitter be used to connect a keypad and another network device to the modbus RTU port on the ATV212 drive?
Issue:
Attempting to connect multiple devices to the Modbus RTU Port.

Product Line:
Altivar 212, ATV21, S-Flex

Environment:
All

Cause:
N/A

Resolution:
No.
The Modbus RTU RJ45 port is only designed to accept one path of signal over the network.
The drive can only have one master on one port.

Schneider Electric Global