{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What can cause High CPU usage on the HMIG5U?
Issue:
What can cause High CPU usage on the HMIG5U?

Product Line:
HMIG5U, HMIG5U2, Magelis iPC

Resolution:
A common cause of high CPU usage on the HMIG5U/HMIG5U2, or Magelis iPC in general, can be attributed to Windows Update running in the background when there is no internet connection. It will constantly try to reach out to the server, even if there is no internet connection. The remedy would be to turn off the Windows Update.

Schneider Electric Global