{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How to create an application displayed in popup with Ecostruxure Machine Scada Expert
ow to create an application displayed like a popup with Ecostruxure Machine Scada Expert (VijeoXL)

In the menu Project / Viewer, unselect the option 'Start Maximum'
Possibity to select the option "menu" or and "Rezise Border"

In the tab "Graphics" of "Project explorer", double click on "Graphic script"
Then add the following command in the Sub Graphic_OnStart()

$SetViewerPos (pos x, pos y, size x, size y)

See video for more details
https://www.youtube.com/watch?v=Ld8iBNJ-DH0​

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.