Issue
Control power specifications of the ION8650 IO expander module
Product Line
ION8650
Environment
Metering application requiring control for the metering devices
Cause
Need to assess burden of IO expander module of the ION8650
Resolution
The power consumption of the 8650 IO Expander is around 2.5 W minimum (typical) and less than 5 W maximum.
Control power specifications of the ION8650 IO expander module
Product Line
ION8650
Environment
Metering application requiring control for the metering devices
Cause
Need to assess burden of IO expander module of the ION8650
Resolution
The power consumption of the 8650 IO Expander is around 2.5 W minimum (typical) and less than 5 W maximum.
Released for: Schneider Electric Global