What is the part number for Lonworks communication card option for ATV212 drives?
Published date:
22 May 2019
Issue:
What is the part number for Lonworks communication card option for ATV212 drives?
Product Line:
Altivar 212, S-Flex with ATV212
Environment:
All
Cause:
option card
Resolution: VW3A21212 is the Lonworks option card.
The ATV21 and ATV212 have different part numbers and option cards for them, and cannot be used interchangeably.
This provides a four-screw terminal block for connection to Lonworks network. Install in place of standard control board that comes mounted in the Altivar 212 drive.
The I/O count is reduce to 3 logic inputs, 1 analog input and 1 NO/NC relay.
**Note: With this card installed, you have to write to this drive with Lonworks. You cannot monitor only.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.