Issue
When running the PSO runtime, the alarms that are typically shown at the top in red are missing. That area is completely blank.

Product Line
PowerSCADA Operation 9.0, 8.2, 8.1
Environment
Runtime
Cause
Schneider Electric Core Service Host service is required to show the alarms in the runtime.
Resolution
Start the Schneider Electric Core Service Host service on the PSE server.
When running the PSO runtime, the alarms that are typically shown at the top in red are missing. That area is completely blank.
Product Line
PowerSCADA Operation 9.0, 8.2, 8.1
Environment
Runtime
Cause
Schneider Electric Core Service Host service is required to show the alarms in the runtime.
Resolution
Start the Schneider Electric Core Service Host service on the PSE server.
Released for:Schneider Electric Global