{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How long can be shielded cables with IEC60034-25 motors when ATV630/930 is used?
If the motor fulfills IEC60034-25, shielded motor cables can be up to 150m without additional filters.

Schneider Electric Global