{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How long can be unshielded cables with IEC60034-25 motorsif ATV630/930 is used?
If the motor fullfil IEC60034-25, unshielded motor cables can be up to 150m without additional filter.

Schneider Electric Global