{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
SEPAM With a CCA634 Sensor Connector : on which SEPAM can I use it ? Sur Quel Sepam Utilise-t-on le CCA634 ?
SEPAM With a CCA634 Sensor Connector : on which SEPAM can I use it ?
Answer :
Current transformer are connected to SEPAM series 20,40,and 80 through CCA630 or CCA634 connector.
Both are inclunding interposing CTs.
CCA630 includes 3 interposing CTs  to connect 2 or 3 phases CTs.
CCA634 includes 4 interposing CTs :
3 to connect 3 phases CTs
1 for the residual current acquisition (CSH30 is now integrated in CCA634 for this function) :
- the sum of the 3 CTs
- an earth/ground CT
A new SEPAM base, adding a connection for Io channel on SubD 9 connector, is needed to accept the CCA634.
THIS NEW FEATURE HAS BEEN IMPLEMENTED STARTING :
series 20 : 1st week of 2003  S/N 0301001
series 40 : week 23 of 2006  S/N 0623001
series 80 : week 29 of 2006 S/N 0629001

As modification is hardware, no firmware update can change the situation for SEPAM made before these dates.

IEDL3

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.