{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
M580 CPU SMTP capability
Issue
M580  CPU SMTP capability

Product Line
M580

Environment
Unity Pro, Control Expert

Resolution
The M580 CPU does not have SMTP capability. Therefore, there is no Send_Email functionality like the M340 CPU .

The M580 CPUs do support the MBP_MSTR and L9_MSTR block. However, for the MBP_MSTR function block, the M580 CPUs only support the following operation codes: 1 = Write data, 2 = Read data, 14 = CIP Explicit Message, 15 = Send Modbus Request, 23 = Read / Write data.

The SMTP protocol is included in CTRL NOC (BMENOC0321). From the user manual, based on predefined events or conditions, messages are created using the DATA_EXCH function block.
This will be the SMTP solution available for M580.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)