{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is there any relevance of computer clock time for Firmware upgrade of device using Ecoreach?
Yes, it is very relevant. Because, while doing the firmware upgrade of the device within smart panel using Ecoreach, Ecoreach validates the integrity of the Signature file (packaged inside the firmware binary file). And if the computer Clock time is dated back to an older date (like before to 2016), the firmware upgrade of the device will fail.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.