{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the PM5000 series meters be used as a gateway?
Issue
Customer would like to verify if there is a model in the PM5000 series that can act as a gateway.

Product Line
PM5110, PM5330, PM5340, PM5560, PM5563

Environment
Product Characteristics

Resolution
The PM5500 series is the only version of the PM5000 series that can be used as a gateway, as they are equipped with both an Ethernet and serial port. This functionality was introduced with firmware version 2.0.1. See FA299853 for how to upgrade the firmware of a PM5500.

The PM5100 and PM5300 series are only equipped with either an Ethernet port or a serial port.