Issue
Adding a BACnet device to the SCADA project requires the BACnet driver to be installed.
Product Line
EcoStruxure™ Power SCADA Operation 8.2
PowerSCADA Expert
Environment
Windows Installer
Cause
Installing BACnet driver and Cimetrics BACstac protocol stack to support the device that communicates through BACnet driver.
Resolution
Adding a BACnet device to the SCADA project requires the BACnet driver to be installed. The following video with depict the process of installing the driver.
Video description:
1. BACnet driver installation
2. BACstac protocol stack installation
3. Removal of virtual port and selection of physical port
4. Correct port selection verification
5. How to modify BACstac using the batch file once installation is finished
NOTE: It is the responsibility of the installer to verify correct version of the BACnet driver is being installed for any specific version of PSE. All versions go through the same installation process.
Adding a BACnet device to the SCADA project requires the BACnet driver to be installed.
Product Line
EcoStruxure™ Power SCADA Operation 8.2
PowerSCADA Expert
Environment
Windows Installer
Cause
Installing BACnet driver and Cimetrics BACstac protocol stack to support the device that communicates through BACnet driver.
Resolution
Adding a BACnet device to the SCADA project requires the BACnet driver to be installed. The following video with depict the process of installing the driver.
Video description:
1. BACnet driver installation
2. BACstac protocol stack installation
3. Removal of virtual port and selection of physical port
4. Correct port selection verification
5. How to modify BACstac using the batch file once installation is finished
NOTE: It is the responsibility of the installer to verify correct version of the BACnet driver is being installed for any specific version of PSE. All versions go through the same installation process.
Released for: Schneider Electric Global