{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can you set up preset speeds on the ATV630 and ATV930 drives?
Issue:
Set up preset speeds on the ATV630 and ATV930 drives.

Product Line:
Altivar Process ATV600 ATV900

Environment:
All

Cause:
Setting up preset Speeds

Resolution:
Under the Main menu, go to Complete Settings > Generic Functions > Preset Speeds > 2 Preset Freq = DIx, then Preset Speed 2 = desired frequency.
Additional preset speeds can be set with > 4 Preset Freq = DIy, then set Preset Speed 3 and 4 as desired.  A total of 16 preset speeds are available. The manual contains a truth table that explains which inputs need to be On/Off for multiple Preset Speeds to work.  See the attached excerpt from the manual.

https://www.se.com/us/en/download/document/EAV64318/

Schneider Electric Global

Attachment(s)
ATV600 Preset Speeds bit table.JPG.jpg [85 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.