{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How to Run a Manual Self-test on your Symmetra PX10-80KVA UPS

Article available in these languages: Spanish

Issue:
How to Run a Manual Self-test on your Symmetra PX10-80KVA UPS

Product line:
Symmetra PX1

Environment:
All Product models, all serial numbers

Cause:
At times it is necessary to perform a battery system test outside normally scheduled intervals

Resolution:
Select "Control" from the main Menu
Select "Do Self Test" and hit enter

Confirm the option by selecting Yes and hitting enter (The test will run for 1 minute)

You can monitor the status of the batteries while the test is running by Hitting Escape to get back to the main menu

Select "Status" from the main menu
Scroll down the list to Battery Voltage.

Make a note of the Actual Battery Voltage and How low it goes during the test. When the test is completed this number will start climbing. Value should be as close to 192v as possible. Lower values indicate the batteries are getting weak.

The following video demonstrates this procedure: