Issue:
ATS22 or ATS48 soft starters to control 12 lead wye delta motor?
Product Line:
ATS22 and ATS48
Environment:
All
Cause:
Application
Resolution:
We have not tested the ATS22 or ATS48 on a 12 lead wye delta motor to say for sure it will work without any issues. In most cases you can wire the output of the soft starter to the delta wires only and it may work. However we do not have any published wiring diagrams or suggested connections for this type of application. Consult with your local Drives Application Engineer for their recommendations.
ATS22 or ATS48 soft starters to control 12 lead wye delta motor?
Product Line:
ATS22 and ATS48
Environment:
All
Cause:
Application
Resolution:
We have not tested the ATS22 or ATS48 on a 12 lead wye delta motor to say for sure it will work without any issues. In most cases you can wire the output of the soft starter to the delta wires only and it may work. However we do not have any published wiring diagrams or suggested connections for this type of application. Consult with your local Drives Application Engineer for their recommendations.
Released for:Schneider Electric Global