{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can we join two expansion cables together between BMXXBE1000 modules
Issue:
Customer needs to add an extension rack to an M340 installation using BMXXBE1000 modules. The distance between racks is around 15metres.
He wants to know if he can join two expansion cables together (e.g. BMXXBC120K & BMXXBC030K) with a standard DB9 joiner (female-female)?

Product Line:
M340, M580, BMXXBE1000

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution::
Yes, this should work, as long as the cumulative length of all the cables used in a PLC station is less than or equal to 30 m.

Schneider Electric Global