{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: APC AV S Type Power Conditioner w/ Battery Back-up - Battery Replacement Procedure
Issue:

UPS requires the replacement of it's internal battery - RBC63


Product Line:

APC AV Power Conditioners w/ Battery Back-UPS


Environment:

UPS is operating Online with a Replace Battery Condition


Cause:

This may be caused by one of the following conditions;
  • Battery Age
  • Battery Damage
  • Improper Battery Connection

Resolution:

The following video details the process for removing and reinstalling the internal Replacement Battery Cartridge.