{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
PME/PSE 8.x: Starting the Floating License Manager in 'Expert' mode
Issue
Starting the floating license manager in expert mode.

Product Line
Power Monitoring Expert 8.x
PowerSCADA Expert 8.x


Environment
Floating License Manager

Cause
Modify and/or delete corrupted PME/PSE licenses.

Resolution
1. Create a shortcut of the 'FloatingLicenseManager.exe' file found at the following default directory:
C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Floating License Manager

2. Right-click on the 'Floating License Manager' shortcut file and select 'Properties'.
Add 'expert' after the following entry in the Target parameter: "C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Floating License Manager\FloatingLicenseManager.exe"
E.g. "C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Floating License Manager\FloatingLicenseManager.exe" expert



3. Click 'OK' in the properties window to apply and save the changes.

Schneider Electric Global